Actualités

Belden Receives Major Recognition from Cabling Installation & Maintenance and Commercial Integrator Magazines

Communications de l'entreprise
Seven Belden cabling and connectivity solutions and projects recognized for innovation.


St. Louis, Missouri – August 31, 2021 –
Belden Inc., a global leader in signal transmission solutions for mission-critical applications, announced today that it has been recognized for being among the best in the industry by two notable awards programs: Cabling Installation & Maintenance’s Innovators Awards and Commercial Integrator and CEPro’s Top New Technology (TNT) Awards. This year, Belden received:

 

Innovators Awards

The Cabling Installation & Maintenance Innovators Awards program reviews and recognizes the most innovative applications of cabling and communications technology products and systems within the structured cabling industry. Honorees were recognized at BICSI’s 2021 Fall Conference on Aug. 22, 2021, in Las Vegas.

 

Platinum Award in the Value-Added Programs category:

  • The Belden Engineering Center for R&D and Innovation-Shanghai plays a vital role in researching and developing mission-critical solutions for Belden’s customers and has world-class equipment to serve cable and connectivity research, new technology development and product innovation. It’s the first lab in the world certified under VDE TDAP Program for listed standards.
  •  

    Gold Awards in the Cabling Media category:

  • Belden’s Ethernet/IP Fire-Resistant Cable & Testing System is designed for unexpected situations like a deep tunnel on fire, where signal transmission systems need to remain functional for long hours so that surveillance systems keep working. The cable stands alone under 842 degrees Celsius of fire for over three hours. During this period, the data transmission is consistent and stable.

     

  • Belden’s OptiTuff™️ Mini Fiber Cables utilize ruggedized thermoplastic material as a cost-effective, top-quality alternative to traditional metal armored cable. They provide superior durability and crush resistance compared to non-armored fiber cables, making them some of the most versatile fiber cables available.

     

    Gold Awards in the Applications and Case Studies category:

  • Belden provided a complete, end-to-end cabling and connectivity solution to support the first indoor-outdoor stadium ever constructed. The cabling infrastructure supports never-before-seen technology, such as a roof-suspended Oculus video board, as well as Wi-Fi 6, digital ticketing and highly sophisticated mobile wireless access.

     

  • Belden provided Digital Electricity™ Cables and connectivity to support the use of Digital Electricity as Circa Resort & Casino Las Vegas’ backbone power distribution infrastructure. This makes it the Strip’s most intelligent building and longer distance capabilities of this cabling enables a guest experience unlike that of any other casino or resort.

     

  • Belden’s 10GXS Category 6A Cables and REVConnect Connectivity were used for PoE LED lighting in Dubuque County’s historic courthouse, 67,000-square-foot Secondary Roads Facility and 10,000-square-foot Dubuque County Office Building. Belden solutions provided fast installation and reliable performance across long distances.

     

    TNT Awards

    The TNT Awards annually recognize new and outstanding products and services exhibited at the Integrated Systems Europe (ISE) show. A team of judges select the top products and services across several commercial and residential categories. Solutions that stand out for offering technological innovation, benefits to integrators and benefits to end-users are honored.

     

    A winner in the Specialty AV Cables or Connectors category:

  • The REVConnect Shielded FlexPlug eliminates compatibility issues when connecting endpoint devices; it works with any IoT device that uses an RJ45 plug. Supporting the award-winning REVConnect termination process, the Shielded FlexPlug can be deployed in applications where a field-terminated plug inhibits direct connection because of size and cable routing constraints.
  •  

    "We are proud and honored to be recognized for our innovation and customer experience," says Ashish Chand, executive vice president, industrial automation at Belden. "Since 1902, we have been focused on making continuous improvements to innovation. We bring together and cultivate the best talents across the business, and we keep investing in research and development, even under difficult times like the global pandemic."

     

    “Being recognized every year is an honor and special accomplishment,” says Julie Furber, executive vice president, smart buildings at Belden. “Our solutions are focused on providing value to end-users and installers. As we find new ways to support their goals, innovation is focal point in that process. We’re thrilled that Cabling Installation & Maintenance, Commercial Integrator and CEPro have recognized these efforts.”

     

    To learn more about these solutions, as well as the types of technology and applications they support, visit www.belden.com.

     

    À propos de Belden 

    Belden Inc., a global leader in high-quality, end-to-end signal transmission solutions, delivers a comprehensive product portfolio designed to meet the mission-critical network infrastructure needs of industrial and enterprise markets. Avec des solutions innovantes visant une transmission fiable et sécurisée de quantités toujours plus grandes de données, d'audio et de vidéo, ce qui est nécessaire pour les applications actuelles, Belden se place au centre du passage de l'humanité à un monde connecté. Founded in 1902, the company is headquartered in St. Louis, USA, and has manufacturing capabilities in North and South America, Europe and Asia. For more information, visit us at www.belden.com; follow us on Twitter @BeldenInc. 

    ###

    Pour plus d’informations, veuillez contacter :

    Lisa Williams
    Responsable communication et marketing
    (317) 815-2402
    lisa.williams@belden.com


    Kate D’Imperio
    Responsable communication et marketing
    (317) 764-9766
    kate.dimperio@belden.com

    Belden, Belden Sending All The Right Signals, and the Belden logo are trademarks or registered trademarks of Belden Inc. or its affiliated companies in the United States and other jurisdictions. Belden et d'autres institutions peuvent aussi avoir des droits de marque au sens des conditions énoncées dans le présent document.